DUG_Odace Rotary Dimmer_WH-03

Setting up the Power On Behaviour

You can set the brightness level of your device when turned On.

  1. On the Home page, tap .

  2. Tap Devices > Lights.

  3. Select the device you want to update and tap Power On Behaviour.

    NOTE: If you are unable to find this option in your app, reset the device to factory default and perform the pairing process.
  4. Select one of the following options as per your preference:

    Last On Brightness Level: The light turns on at the same brightness as when it was last turned Off.

    Specific Brightness Level: This option allows you to get the desired brightness level every time you turn On the light. Drag the slider bar to set the brightness.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?