DUG_Odace Rotary Dimmer_WH-03

Switching/Dimming the device manually

You can manually turn on/off the dimmer and increase/decrease brightness level. This will provide power to the load connected to it.
To turn on or off the dimmer, short-press the push button (< 0,5 s).

To increase brightness, turn the dimmer knob clockwise, and to decrease brightness, turn it anti-clockwise.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?