Setting Tariff
You can set the tariff based on your contract type:
-
Flat rate: Flat rate is defined as the fixed rate for the entire time period of electricity service. Configuring - flat rate.
Peak/Off-Peak Hours rate: Peak rate is defined as a rate set to a specific period of time at which electrical consumption is at its highest. Off peak rate is the time period when the demand for power is at its lowest. It is the amount you pay for each unit of electricity consumed for the time period set. Refer to Configuring - peak rate.
-
No contract: Electricity rate is not set, no information related to bill will be shown in the app.
NOTE: By default, No Contract option is set. -
Feed in tariff:
IMPORTANT: Feed in tariff will be shown only if you have set the PowerTag for Solar or Solar and Battery which feed electricity to the Grid.The electricity generated from solar or solar and battery that is not used is exported to the electricity grid. You are eligible for a payment for the exported electricity. This payment is called a feed-in tariff. Refer to Configuring - feed in tariff.NOTE: You can see the tariff data based on your local currency.
Once PowerTag is commissioned and the contract limit is set, user gets notified that this feature is available. The Tariff Entry screen appears on the Home page.