Showing 1,191 - 1,200 of 1,622 results

Page 120 of 163
  • Termostato Empotrado Wiser 2 A Guía del usuario del dispositivo Wiser Home

    calefacción de la pestañaControl. • Añadiendo el termostato a sus Favoritos. Para obtener másinformación sobre Favoritos, consulte el tema Gestión de favoritosen la correspondiente guía del usuario del sistema. SUGERENCIA: Al pulsar se puede ajustar el tiempo de Boost ydespués se apaga cuando termina el
  • EcoWatt User Guide

    Mode Good night Tips and advice See all Stay safe and simulate your presencewith lights and shutters when you areaway for added security Show me Not for me National Electrical Grid is operating normallyWhat's new? Eco Watt Eco Watt will provide you with the live andforecasted status of the grid and
  • Airzone Plenum and Aidoo Pro - Air conditioner

    remove the device from the Wiser system. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Away Mode Away Mode Away mode allows you to configure your devices even when you are away from home. For example, you can set the
  • Wiser Home System User Guide (Belgium)

    Edit Pool PumpEnergy centre ON GridEnergy centre Importing 10.11 kW Moments Away Mode and reduce temperatures to boost yoursavings whenever you leave home Save with away mode Show me Not for me Automations 52 SUG_NL_WH-04 Configuring the Wiser System 1. On the App Settings, page 52, click on Support.2
  • Wiser Home

    Joseph Monier 92500 Rueil-Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Modes Modes Schneider Electric 35 rue Joseph Monier 92500 Rueil-Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Mode Absence Mode Absence Schneider Electric 35 rue Joseph Monier 92500 Rueil-Malmaison France + 33 (0) 1 41 29
  • Managing shutter operation without temperature sensor

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    reference temperature: In the Seasonal Comfort Mode set-up page, tap Other room sensors. Wiser Home app displays the rooms without temperature sensors in list (A). Select a room from the list (A). You can use one of the following temperatures as a reference temperature for the selected room: Temperature
  • Managing shutter operation without temperature sensor

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    reference temperature: In the Seasonal Comfort Mode set-up page, tap Other room sensors. Wiser Home app displays the rooms without temperature sensors in list (A). Select a room from the list (A). You can use one of the following temperatures as a reference temperature for the selected room: Temperature
  • Modo de carregamento

    Schneider Charge – Guia do utilizador do dispositivo Wiser Home

    carregamento. No menu EV Charging Mode, selecione uma das seguintes opções: Manual: Para iniciar o processo de carregamento imediatamente após a ligação à tomada de um veículo elétrico. Reduzir a minha fatura: Para iniciar automaticamente o carregamento durante a próxima ranhura rentável disponível, com
  • Setting the room temperature manually

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    decrease the temperature setpoint. In P3, P5, P6 presets, if floor sensor is fitted, device will be in room temperature with floor limits mode. When the room temperature is at or above the current setpoint, the floor temperature is below the lower floor temperature limit (min. guard), the demand is
  • Configuration de l’appareil

    Unica - Variateur rotatif universel connecté – Guide de l'utilisateur de l'appareil domestique Wiser

    l’emplacement. C Mode RL-LED: Vous pouvez améliorer la qualité de la variation dans l’application en cas de problèmes de lumière vacillante. Appuyez sur l’interrupteur à bascule pour activer le mode RL-LED. Consultez Caractéristiques techniquespour plus d’informations. D Comportement des témoins LED
Page 120 of 163