Showing 121 - 130 of 328 results

Page 13 of 33
  • Creating an automation

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more
  • Creating an automation

    LK FUGA Wiser Multiwire LED Rotary Dimmer – Wiser Home Device User Guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Creating an automation

    Ovalis - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more information about Away Mode, refer to the
  • Creating an automation

    Exxact - Connected Single Socket Outlet 16A – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more information about Away Mode, refer to the
  • Creating an automation

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more
  • Creating an automation

    Unica - Connected Universal Push-button Dimmer LED – Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Creating an automation

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more
  • Insights

    Wiser Home – System User Guide (UK, Ireland)

    saved for the current month, along with a 3-month average comparison. It also provides data on hours saved in Away Mode and allows you to enable Eco Mode for additional savings. C Tracks adjustments made to heating, including the number of times the heating was turned up or down, as well as
  • Odace - Connected Thermostat 2 A Wiser Home Device user guide

    occupancy duration. When presence detect or setback has been activated, thermostat dot matrixdisplay shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° CCelsius and the inputs detect room occupancy, the thermostat will adhere
  • EcoWatt User Guide

    isavailable. The Ecowatt screen appears on the Home screen. 1. Read the feature update and swipe to navigate to next screen. 2. Tap to close the overlay screen. Control InsightHome Automations Good evening Favourite devices Edit ShutterLiving room Open Motion SensorHallway Unoccupied Moments Edit Away
Page 13 of 33