Showing 121 - 130 of 1,647 results

Page 13 of 165
  • Gestion de la fonction délestage

    Mureva EVlink – Guide de l'utilisateur de l'appareil domestique Wiser

    spécifications de votre contrat, il est donc important de consulter la section Setting Tariff pour obtenir des informations sur les tarifs heures pleines et heures creuses. Les appareils éligibles seront automatiquement intégrés au système de gestion de la fonction délestage, ce qui optimisera davantage la
  • Creating an automation

    Wiser Smart Plug 16A – Wiser Home Device User Guide

    Away mode. Energy price changes: To define the energy price limit. This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. Maximum 10 conditions can be added. To remove an added condition, swipe left and tap . To set a specific time for your
  • Gestion de la fonction délestage

    Wiser Prise Intelligente – Guide de l'utilisateur de l’appareil Wiser Home

    spécifications de votre contrat, il est donc important de consulter la section Setting Tariff pour obtenir des informations sur les tarifs heures pleines et heures creuses. Les appareils éligibles seront automatiquement intégrés au système de gestion de la fonction délestage, ce qui optimisera davantage la
  • Creating an automation

    Wiser Plug – Wiser Home Device User Guide

    Away mode. Energy price changes: To define the energy price limit. This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. Maximum 10 conditions can be added. To remove an added condition, swipe left and tap . To set a specific time for your
  • Creating an Automation

    Wiser Home – System User Guide (Sweden, Finland)

    automation based on changes in energy prices. This trigger is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. The system manages electricity pricing at a precision of 0.01 €/kWh. Example: The daily average electricity price is 0.24 €/kW. You have set your
  • Creating an Automation

    Wiser Home – System User Guide (Denmark)

    automation based on changes in energy prices. This trigger is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. The system manages electricity pricing at a precision of 0.01 €/kWh. Example: The daily average electricity price is 0.24 €/kW. You have set your
  • Wiser Home

    92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Setting Tariff Setting Tariff You can set tariff in the Wiser Home app to access your energy cost and billing data. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Configuring
  • Wiser Home

    seamless look. You can also personalize the app experience by selecting your preferred appearance to light mode or dark mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Setting Tariff Setting Tariff You can set tariff in the Wiser Home app to
  • Insights

    Wiser Home – System User Guide (Belgium)

    Insights Insights Insights The Insights provides information on the annual bill for the tariff set. It helps to keep track of your energy. The option to set a tariff is only available if you have an Energy device installed in your home. For more information, please refer to the Device User Guide of
  • Wiser Power Micromodule

    29 70 00 www.se.com Schneider Electric Setting the device location Setting the device location Using the Wiser Home app, add the module to any room (such as living room, bedroom etc). Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider
Page 13 of 165