clignote en rouge. Les appareils d'éclairage connectés clignotent en fonction del'identification réussie du variateur. Différents modes de connectivité Affichage LED Statut La LED clignote en vert et en rouge lors de l’appairage. L’appareil tente de se connecter à un autre mode de
, som f.eks. lagerrum eller ubenyttede rum.• Tilsluttet termostat 2 A (til forudindstilling af P1 og P2)• Tilsluttet termostat 16 A (til alle forudindstillede)• Smart ZB termostat 16 A Identifikation af enhedenMed app'en Wiser Home kan du identificere gulvvarmen fra andre tilgængeligeenheder i
referred to as Puck) combines theadvantages of smart dimmer functionality with ordinary mechanical push-buttonswitches. It transforms a conventional switch into a connected device which canbe controlled from the switch or through the Wiser app. It can switch and dim theohmic, inductive, or capacitive
. This can be useful if there are areas in a building that do notrequire cooling, such as storage rooms or unoccupied spaces.• Connected Thermostat 2 A (for Preset P1 and P2)• Connected Thermostat 16 A (for all Preset)• Smart ZB Thermostat 16 A Identifying the deviceUsing the Wiser Home app, you can
. The device can be configured through the Wiser Home app. Advantage of using a Wireless switch:• Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones.• Easy to install on the wall: no wiring
Gebäude gibt, für die keine Kühlungerforderlich ist, z. B. Lagerräume oder nicht belegte Bereiche.• Connected Raumtemperaturregler 2 A (für Preset P1 und P2)• Connected Raumtemperaturregler 16 A (für alle Preset-Modelle)• Smart ZB Temperaturregler 16 A Identifizierung des GerätsMit der Wiser Home
on E.g. if the motion is detected Activate a momentE.g. enable Away mode WaitE.g. wait 10 mins until next action All Living Room Kitchen Bedroom Please select the devices you want to addto this moment. Select devices Smart Socket Radiator Relay switch Living Room Bedroom Blind control switch Kitchen
)• Termostato conectado 16 A (para todas as predefinições)• Termostato Smart ZB 16 A Identificar o dispositivoUtilizando a aplicação Wiser Home, pode identificar o Controlador de pisoradiante a partir de outros dispositivos disponíveis na divisão.Para identificar o Controlador de piso radiante: 1. No
Puck CCT5010-0003 Om enhedenWiser Multiwire mikromodul-lysdiodelysdæmperen (herefter kaldet lysdæmper/mikromodullysæmper) kombinerer fordelene ved smart lysdæmperfunktion medalmindelige mekaniske trykknapafbrydere. Den transformerer en almindeligkontakt til en tilsluttet enhed, som kan styres med
switch:• Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones.• Easy to mount on the wall: no wiring required.Features of a Wireless Switch:• Add various actions (such as lighting/shutter control) to