Showing 1,291 - 1,300 of 9,870 results

Page 130 of 987
  • Account settings

    Wiser Home – System User Guide (Germany, Austria)

    Account settings Account settings Account settings In the account menu you can manage your address, customize notifications and alarms, manage privacy, connect third-party apps, update your password, and even delete your account when needed. In the Settings menu: Tap Account (A). The Account menu
  • Account settings

    Wiser Home – System User Guide (Spain and Portugal)

    Account settings Account settings Account settings In the account menu you can manage your address, customize notifications and alarms, manage privacy, connect third-party apps, update your password, and even delete your account when needed. In the Settings menu: Tap Account (A). The Account menu
  • Account settings

    Wiser Home – System User Guide (UK, Ireland)

    Account settings Account settings Account settings In the account menu you can manage your address, customise notifications and alarms, manage privacy, connect third-party apps, update your password, and even delete your account when needed. In the Settings menu: Tap Account (A). The Account menu
  • Rollen in der Wiser Home-App

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    einstellen Ja Ja Benachrichtigungen zur Auslösung von Moment/Automatisierung erhalten Ja Ja Als Professioneller Installateur können Sie mit der App ein Wiser-System einrichten und Geräte hinzufügen, ohne dass Sie angemeldet sein müssen. Jeder Benutzer kann sich bei der App anmelden, wenn der Hauseigentümer
  • Wiser Window/Door Sensor Wiser Home Device user guide

    the automation.– Activate a moment: Select the moment that you want to trigger.– Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to amaximum of 24 hours. This feature is useful for delaying actions within
  • Capteur de température/humidité Wiser Guide de l'utilisateur de l’appareil Wiser Home

    the automation.– Activate a moment: Select the moment that you want to trigger.– Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to amaximum of 24 hours. This feature is useful for delaying actions within
  • Rôles dans l’application Wiser Home

    Wiser Home – Guide de l’utilisateur du système (France)

    appareils à des moments / automatismes Oui Oui Adapter des paramètres d’appareils à des moments / automatismes Oui Oui Définir des conditions de déclenchement dans des moments / automatismes Oui Oui Recevoir des notifications de déclenchement de moment / automatisme Oui Oui L’application propose à
  • Substituir a bateria

    Sistema M e Sistema D - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    Substituir a bateria Substituir a bateria Substituir a bateria Substitua a bateria do dispositivo quando o nível estiver baixo ou perigosamente baixo. É possível ver o nível da bateria na aplicação. Siga os passos para substituir a bateria do dispositivo: PERIGO DE QUEIMADURA QUÍMICA Manter as
  • Deleting a schedule

    Wiser Micro Module Light Switch – Wiser Home Device user guide

    Deleting a schedule Deleting a schedule Deleting a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to delete. Tap SCHEDULE DETAILS, tap Delete, and then select OK.
  • Adding a Schedule

    Wiser Home – System User Guide (France)

    Adding a Schedule Adding a Schedule Adding a Schedule On the Automation Screen (A), tap (B) icon. Enter a name in the text field (C). Select the Device type of the Schedule. A Schedule can only be created for one Device type. If you want to switch a light at the same time as closing a blind, you
Page 130 of 987