Showing 131 - 140 of 328 results

Page 14 of 33
  • Troubleshooting in Quick Home Connect

    LK FUGA Wiser Multiwire LED Rotary Dimmer – Wiser Home Device User Guide

    Rotary dimmer Wiser Wireless switch not able to control the device reliably. The Wiser Wireless switch and the device are too far away from each other. Place the Wiser Wireless switch in a position closer to the device. The Wiser Wireless switch lost pairing. Pair the device again. Refer to Rotary
  • Wiser Plug Device user guide

    ) signal range extender to control yourelectrical appliances remotely. It has a built-in RF signal range extender to enableconnectivity to devices further away from the Wiser Hub. Advantage of using the Plug:• Configure several time schedules to switch on/off the Plug.• Set notification to alarm when
  • Wiser Radiator Thermostat

    Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Boost All Boost All You can apply a boost of +2 °C for 1 hour to every room in the system. It won’t affect hot
  • Troubleshooting in Quick Home Connect

    Unica - Connected Relay Switch 10 A – Wiser Home Device user guide

    switch Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Relay switch The Wireless switch battery
  • Troubleshooting in Quick Home Connect

    Exxact - Connected Single Socket Outlet 16A – Wiser Home Device user guide

    outlet Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Socket outlet The Wireless switch
  • About the device

    Wiser Plug – Device user guide

    devices further away from the Wiser Hub. Advantage of using the Plug: Configure several time schedules to switch on/off the Plug. Set notification to alarm when power consumption (high or low). Features of the Plug: Mobile or manual control anytime, anywhere with the Wiser app Works with Amazon Alexa, the Google Assistant and Siri Diagram of operating elements A. On/Off button
  • System M and System D - Connected Thermostat 2 A, ZB Wiser Home Device user guide

    away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° CCelsius and the inputs detect room occupancy, the thermostat will adhere to the23° C setpoint. However, if the room becomes unoccupied, the thermostat willmaintain the 23° C
  • Troubleshooting in Quick Home Connect

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    control switches Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Blind control switches The
  • Creating an automation

    PowerTag Control – Device user guide

    based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): The Away Mode is intended to set your Home to a practical state for longer absences, such as leaving for the weekend. Maximum 10 conditions can be added. Select
  • Airzone Plenum and Aidoo Pro - Air conditioner Wiser Home Device user guide

    Wiser System (Parent Topic) • Setting the device location • Removing the device from the Wiser system • Away Mode Setting the device locationYou can change the device location using Wiser Home app (such as bedroom,living room, dining room etc.). 1. On the Home screen, tap . 2. Tap Devices, select the
Page 14 of 33