Showing 1,391 - 1,400 of 1,648 results

Page 140 of 165
  • Creating a moment

    Unica - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    -right screen. After setting all conditions, tap Save. Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it. If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Moments toggle switch. You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.
  • Creating a moment

    Wiser Multiwire Micro Module LED Dimmer – Wiser Home device user guide

    , select Micromodule dimmer. Tap (D) to turn on. Drag the sliding bar up/down to increase/decrease the brightness (E) and tap Set on the upper right corner. After setting all conditions, tap Save. Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it. If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Momentstoggle switch.
  • Creating a moment

    Exxact - Connected Multiwire Universal Rotary Dimmer LED – Wiser Home Device user guide

    -right screen. After setting all conditions, tap Save. Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it. If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Moments toggle switch. You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.
  • Creating a moment

    LK FUGA Wiser Multiwire LED Rotary Dimmer – Wiser Home Device User Guide

    -right screen. After setting all conditions, tap Save. Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it. If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Moments toggle switch. You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.
  • Using the device

    LK FUGA® Wiser wireless PIR with relay – Wiser Home Device user guide

    /off. B Displays the current Lux value of the light present in the room. C Tap to open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. D Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite
  • Unica - Toma de corriente inteligente, 1 elemento, 16 A

    sistema por debajo de un límite definido. El valor límite lo establece la potencia contratada, consulte Setting Tariff. Los dispositivos que cumplan con los requisitos se añadirán automáticamente a la gestión de cargas. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison Francia +33 (0) 1
  • Renova - Connected Thermostat Room/Floor 16 A Wiser Home Device User Guide

    ..............................................................20Advanced device settings ....................................................................21Floor sensors settings .........................................................................24Room setting
  • eSetup App

    Wiser Home – System User Guide (France)

    individual Devices. You can test the Devices. To configure a Device: Choose the Device type (Light and Shutter Devices). Choose the specific Device type, e.g. rotary dimmer. Connect the Device to the app by setting it into pairing mode. The app will show you how to set the Device into pairing mode. Set the Name for the Device. Assign the Device to a Room. Test the Device.
  • Pairing the device with the Wiser Hub

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    slats: Proceed to step 8 and step 10. Tap Shutter Next and enter the open/close duration of shutter. Refer to Setting default run time. Tap Shutter with tilting slats Slat Type, select a slat type and tap Set: Horizontal Tilted Vertical Tap Next and enter the following durations: Open duration
  • Floor sensors settings

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    temperature ranges from -9°C to +9°C and can be adjusted in 0.1°C increments. Tap Save. Floor sensor limit To set the upper and lower temperature limit: On setting page, tap Floor Sensor Upper Limit to set upper temperature limit of the floor sensor and then tap Save. The temperature ranges form 5
Page 140 of 165