Showing 1,411 - 1,420 of 9,870 results

Page 142 of 987
  • Editing a schedule

    Odace - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    Editing a schedule Editing a schedule Editing a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to edit. Tap the SCHEDULE DETAILS and you can do the following actions: Rename the schedule (A). Within the Applies to (B) menu, you have the option to select from the
  • Operating a Dimmer

    Odace - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    Operating a Dimmer Operating a Dimmer Operating a Dimmer You can switch the dimmer ON/OFF and adjust its brightness using the paired Wireless switch. Short press the top (ʌ+) or bottom (v-) of the Wireless switch (< 0,5 s) to turn ON/OFF the connected load (A). Long press the top (ʌ+) or bottom (v-) of the Wireless switch (> 0,5 s) to increase or decrease the brightness of the connected load (B).
  • Deleting a schedule

    Odace - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    Deleting a schedule Deleting a schedule Deleting a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to delete. Tap SCHEDULE DETAILS, tap Delete, and then select OK.
  • Adding a Schedule

    Wiser Home – System User Guide (Spain and Portugal)

    Adding a Schedule Adding a Schedule Adding a Schedule On the Automation Screen, tap (A) icon. Enter a name in the text field (C). Select the Device type of the Schedule. A Schedule can only be created for one Device type. If you want to switch a light at the same time as closing a blind, you will
  • Deleting a schedule

    PowerTag Control – Device user guide

    Deleting a schedule Deleting a schedule Deleting a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to delete. Tap SCHEDULE DETAILS, tap Delete, and then select OK.
  • Adding a Device

    Wiser Home – System User Guide (Sweden, Finland)

    Adding a Device Adding a Device Adding a Device You can add a new Device at any time. The hub must be installed before adding a Wiser device. Add mains-powered devices before battery-powered devices. Refer to Selecting the mounting location. The instructions provided for adding the device are
  • Editing a Schedule

    Wiser Home – System User Guide (Denmark)

    Editing a Schedule Editing a Schedule Editing a Schedule In the Schedule details screen: Tap (A) icon to change the name of the Schedule. Select the Devices (B) the Schedule applies to. Select the day (C) you want to add or edit events. Tap (D) icon to edit an event. Tap (E) icon to add an event to
  • Adding a Room

    Wiser Home – System User Guide (UK, Ireland)

    Adding a Room Adding a Room Adding a Room You can add a new Room when assigning a Device or from the List of Rooms: Tap (A) icon. Enter a name in the text field (B). Tap Submit (C)
  • Editing a schedule

    Exxact - Connected Multiwire Universal Rotary Dimmer LED – Wiser Home Device user guide

    Editing a schedule Editing a schedule Editing a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to edit. Tap the SCHEDULE DETAILS and you can do the following actions: Rename the schedule (A). Within the Applies to (B) menu, you have the option to select from the
  • Editing a Schedule

    Wiser BMS – Building Management System – User Guide

    Editing a Schedule Editing a Schedule Editing a Schedule Select a room in the floorplan layout. The selected room screen appears. Click Schedule. The Wiser Schedule screen appears. On the Wiser Schedule screen, select the day and click . Change the Temperature (A) or When (B). Click Set (C) to save the event.
Page 142 of 987