+ 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider Electric 35 rue Joseph
Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Adjusting the brightness level using app Adjusting the brightness level using app Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500
+ 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider Electric 35 rue Joseph
triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. e.g. Good
Home ConnectPairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quicksuccession. LED blinks green, once per second. Pairing mode is active for 60 seconds. Whenpairing is completed, LED stops blinking. Troubleshooting in Quick Home Connect Symptom
Creating an automation The following is an example of creating an automation to boost for few hours when the heater is set to certain temperature. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric 35 rue Joseph Monier 92500 Rueil
www.se.com Réglage du niveau de luminosité à l’aide de l’application Réglage du niveau de luminosité à l’aide de l’application Schneider Electric 35 rue Joseph Monier 92500 Rueil-Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Mode Absence Mode Absence Schneider Electric 35 rue Joseph Monier
, l’appareil est en mode de programmation manuelle. • Wiser Home IA : Cette fonctionnalité planifie automatiquement vos chargeslorsque le coût est le moins élevé. Reportez-vous à Wiser Home IA. • Plage Horaire personnalisée : Vous pouvez créer votre propre programmepour activer ou désactiver votre
Wiser trådløs jalousi styring for indbygning (puck) – Brugervejledning til Wiser Home-enheden
enheden med trådløse kontakter og Wiser Hub, opsætter tidsplaner, skaber automatiseringer og øjeblikke og kalibrerer lukkerbevægelser. Brugerne kan tilpasse enhedens indstillinger, omdøbe og flytte enheder og styre lukkeren manuelt eller via en app. Guiden dækker også Seasonal Comfort Mode, som justerer
information provided by the TIC. The EVlink Home Smart is configured in Mode 1. You can enable or disable the communication between the EVlink Home Smart and the TIC device. Tap Continue in the Supervision page. Once all the device settings are configured, tap Handover to customer and share the PIN with