Showing 1,471 - 1,480 of 9,870 results

Page 148 of 987
  • Operating a Shades Control

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    Operating a Shades Control Operating a Shades Control Operating a Shades Control You can operate the shades control using the Wireless switch. Long press the Wireless switch (> 0,5 s) to move the shades control up or down. Press (ʌ+) to open the shades control (A) Press (v-) to close the shades
  • Reduzir a minha fatura

    Micromódulo de potência Wiser – Guia do utilizador do dispositivo

    Reduzir a minha fatura Reduzir a minha fatura Reduzir a minha fatura Utilize a aplicação Wiser Home para ver o controlo e as programações dos dispositivos. A funcionalidade Reduzir a minha fatura programa automaticamente os dispositivos de elevado consumo de energia para funcionarem durante as
  • Operating a Relay Switch

    Exxact - Connected Relay Switch 10 A – Wiser Home Device user guide

    Operating a Relay Switch Operating a Relay Switch Operating a Relay Switch You can turn the light on/off using the paired Wireless switch. Short press the top or bottom of the Wireless switch (< 0,5 s) to turn on/off the light.
  • Operating a Relay Switch

    Exxact – Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Operating a Relay Switch Operating a Relay Switch Operating a Relay Switch You can turn the light on/off using the paired Wireless switch. Short press the top or bottom of the Wireless switch (< 0,5 s) to turn on/off the light.
  • Setting up a schedule

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The shutter can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time. The devices can be fully controlled by schedule
  • Operating a Relay Switch

    LK FUGA Wiser Push-button Switch – Wiser Home Device user guide

    Operating a Relay Switch Operating a Relay Switch Operating a Relay Switch You can turn the light on/off using the paired Wireless switch. Short press the left or right of the Wireless switch (< 0,5 s) to turn on/off the light.
  • Setting up a schedule

    LK One Wiser Multiwire LED Rotary Dimmer – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The dimmer can be fully controlled by a schedule. Once the schedule is set, the dimmer operates at a given time. On the Home screen, tap . Go to Schedules > to create a schedule. Enter the name of the schedule (A). In the TYPE
  • Setting up a schedule

    Exxact - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The Motion Sensor Switch can be fully controlled by a schedule. Once the schedule is set, the Motion Sensor Switch operates at a given time. On the Home screen, tap . Go to Schedules and tap to create a schedule. Enter the name of
  • Wiser Temperature/Humidity Sensor

    . If the room has multiple temperature measuring devices such as the Wiser Room Thermostat, Connected Flush-mounted thermostat, or Temperature/Humidity Sensor, the system automatically calculates the average temperature from all devices. This ensures that heating is regulated based on a more
  • Wiser Smoke Alarm - 230 V

    without Wiser Hub Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Disconnecting a secondary device Disconnecting a secondary device Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00
Page 148 of 987