Showing 1,491 - 1,500 of 1,648 results

Page 150 of 165
  • Wiser Prise Intelligente Guide de l'utilisateur de l’appareil Wiser Home

    par le PCM. Vous pouvez inscrire jusqu'à huit charges à lafois, ce qui permet de maintenir la consommation totale du système en dessousde la limite établie. Cette limite est déterminée par les spécifications de votrecontrat, il est donc important de consulter la section Setting Tariff pour obtenir
  • Device Details

    Wiser Home – System User Guide (Germany, Austria)

    Device Details Device Details Device Details You can find all relevant settings of a Device in the Device details. You can navigate to the Device details from the List of Devices by tapping the Device or from the Device control by tapping the device setting. A Tap to change the name of the device
  • Troubleshooting

    EVlink Home Smart – Wiser Home device user guide

    correctly or not for EVlink Home Smart with TIC function. Device not removed from the system Hub disconnected from the network. (Applicable only for users with EVlink Home Smart and Wiser hub installed together) Charger unavailable. Device connected to another home network. Try setting up the device
  • Device control

    Wiser Home – System User Guide (Sweden, Finland)

    , will be controlled like any other Device, but need to be set up properly. Detailed information about setting up Climate devices can be found in chapter Climate control. On the Home screen, tap Control tab . You can also set your Control tab as your default landing screen. To do this, go to Home Screen
  • Device control

    Wiser Home – System User Guide (UK, Ireland)

    , will be controlled like any other Device, but need to be set up properly. Detailed information about setting up Climate devices can be found in chapter Climate control. On the Home screen, tap Control tab . You can also set your Control tab as your default landing screen. To do this, go to Home Screen
  • Exxact - Connected Multiwire Universal Push-button Dimmer LED Wiser Home Device user guide

    .............................................. 11 Pairing the device with the Wiser Hub ........................................................12Configuring the device ..............................................................................15 Setting the device location
  • Device presetting

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    floor limit sensor) 10 *Cycle time: This setting determines the length of each on/off cycle of the output relay. The percentage of time within that cycle time that the relay is on is varied based on demand. A longer cycle time may be more appropriate for slow heating surfaces, such as a concrete floor
  • Climate control

    Wiser Home – System User Guide (Sweden, Finland)

    be available. H Add or remove the device from Favourite devices. Refer to Managing Favourites J Navigate to the Room Details of the room to which the climate control is assigned. Setting up a Climate Control While setting up your Climate Control, make sure to consider the following information
  • Wiser Motion Sensor Wiser Home Device user guide

    ...................................................................13Setting the device sensitivity ................................................................14Setting detection delay ........................................................................15Defining Lux setting
  • Wiser 16 A Relay for Temperature Control Wiser Home Device user guide

    > Climate > 16A Relay > Name (A) to rename the device.NOTE: Type and icon (B) are both assigned automatically, based onwhether you have radiators or floor heating. You will be able to view thisonly after the pairing is completed. Setting the device locationUsing the Wiser Home app, you can assign the
Page 150 of 165