step to rename the Socket outlet: 1. On the Home page, tap icon. 2. Tap Devices > Connected Socket > Device Name (A) to rename the Socketoutlet. Delete Identify Device Name Connected Socket OPTIONS Location Device Details A Device user guide_00 9 SysM/SysD - Connected Single Socket Outlet 16 A Setting
Alarm-Battery Setting up connection without Wiser Hub Interconnecting devices without Wiser HubThe smoke alarms can be connected directly to each other via RF connectionseven without a Wiser Hub network. IMPORTANT: Turn the power switch to ON position on all the devices.1. Identify a smoke alarm and
, you can rename the sensor by tapping on the Controltab, Water Leakage Sensor > Device settings > Device Name (A). Setting the device locationYou can add your device to any room (such as bedroom, living room, dining roometc.). 1. On the Home screen, tap . 2. Tap Devices, select the device from the
........................................................10Configuring the device ..............................................................................19 Setting the device location ...................................................................20Advanced settings
before making anychanges to these fields. Add Devices Lights Shutters AppliancesAll Room Thermostat Aidoo Pro Heat Pump If you are setting up a mains powered device, such Climate CLIMATE Airzone Plenum Radiator Thermostat 16A Relay Aidoo Pro Air Conditioner Beta Feature for commercial release. No
screen allows you to configure the device settings according to your preferences. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Setting the device location Setting the device location You can add your device to any room
(A). Setting the device locationYou can add your device to any room (such as bedroom, living room, dining roometc.). 1. On the Home screen, tap . 2. Tap Devices, select the device from the list for which you wish to change thelocation. 3. Tap Location to open setup screen. Window/Door Sensor Delete