klara får användaren ett meddelande om att den härfunktionen är tillgänglig. Skärmen Anti-Tripping visas på startskärmen. SUG_SV_FI_WH-04 185 Styra Wiser-systemet https://www.productinfo.schneider-electric.com/wiser_home/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=SETTING+TARIFF https
-Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Example of an automation Example of an automation This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C. Schneider Electric
..............................................26 Pairing the device with the Wiser Hub ........................................................27Configuring the device ..............................................................................31 Setting the device location
..............................................22 Pairing the device with the Wiser Hub ........................................................24Configuring the device ..............................................................................28 Setting the device location
temperature E 4 UG_EcoWatt_WH_01 EcoWatt Setting EcoWatt alertsYou can set the alert type of your choice. 1. On the Home screen, tap > Account > Notifications and Alarms >National Electrical Grid Status. 2. Enable/Disable the toggle switch (A) to set the notification of your choice.NOTE: All
automation This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison Francia +33 (0) 1 41 29 70 00 www.se.com Schneider Electric Edición de una
switch or throughthe Wiser app. It can switch ohmic, inductive or capacitive loads. NOTE: Do not control any devices that depend on a permanent power supply.Additional features:• Remote controlled with maximum of 10 mechanical push-buttons.• Setting a time schedule via Wiser Home app. Installing the
..............................................20 Pairing the device with the Wiser Hub ........................................................21Configuring the device ..............................................................................25 Setting the device location
..............................................24 Pairing the device with the Wiser Hub ........................................................25Configuring the device ..............................................................................29 Setting the device location
=setting+tariff 12 DUG_Wiser_Airzone_WH-05 Acerca de Plenum Airzone y el sistema Wiser Configuración del dispositivo Ajuste de la localización del dispositivoPuede cambiar la localización del dispositivo (como dormitorio, sala, comedor,etc.) usando la aplicación Wiser Home. 1. En la pantalla Inicio, toque