Showing 181 - 190 of 1,429 results

Page 19 of 143
  • Odace - Connected Thermostat 2 A Wiser Home Device user guide

    occupancy duration. When presence detect or setback has been activated, thermostat dot matrixdisplay shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° CCelsius and the inputs detect room occupancy, the thermostat will
  • LK FUGA® Wiser wireless dimmer Wiser Home Device User Guide

    . Away Mode Boost All Cancel all overrides Bienvenue Balcony Movie night Movie night Push Button 2 Back DUG_LK FUGA Wiser wireless dimmer_WH-00 21 LK FUGA® Wiser wireless dimmer https://www.productinfo.schneider-electric.com/wiser_home/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term
  • Wiser Flush-mounted Thermostat 2 A Wiser Home Device user guide

    setpoint.Refer room settings, page 25 for more information on occupancy duration. When presence detect or setback has been activated, thermostat dot matrixdisplay shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° CCelsius and the
  • Airzone Plenum and Aidoo Pro - Air conditioner Wiser Home Device user guide

    screen, tap . 2. Tap Devices > Climate. 3. Select the device to be removed from the list. 4. Tap Delete (A). 5. Tap Ok after reading the confirmation message. Away ModeAway mode allows you to configure your devices even when you are away fromhome. For example, you can set the temperature and turn on/off
  • Creating an automation

    LK FUGA® - Wiser wireless socket outlet 1½ M – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more information about , refer to the system user
  • Exxact - Connected Motion Sensor with Switch 10 A Wiser Home Device user guide

    single devicein the Wiser System. All functions will be accessible through the Homescreen. Away ModeAway Mode automatically turns off the Motion Sensor Switch. For example, whenyou are away from home for a long time, the light should not turn on due to falsemotion detections. This feature ensures the
  • Wiser Home System User Guide (Denmark)

    InsightHome Good evening Favourite devices Edit Motion SensorHallway Critical battery Unoccupied Moments Edit Away Mode Good night Tips and advice See all Stay safe and simulate your presencewith lights and shutters when you areaway for added security Show me Not for me ShutterLiving room Openuntil 16:00
  • System M and System D - Connected Thermostat 2 A, ZB Wiser Home Device user guide

    setpoint.Refer room settings, page 25 for more information on occupancy duration. When presence detect or setback has been activated, thermostat dot matrixdisplay shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° CCelsius and
  • System M and System D - Connected Thermostat 16 A, ZB Wiser Home Device user guide

    detect or setback has been activated, thermostat dot matrixdisplay shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° CCelsius and the inputs detect room occupancy, the thermostat will adhere to the23° C setpoint. However
  • Création d’un automatisme

    Climatiseur Airzone Plénum et Aidoo Pro – Guide de l'utilisateur de l’appareil Wiser Home

    appareil(E) qui définira la condition. Si vous avez sélectionné la condition comme Mode Absence et agir en tant que Contrôler un appareil alors cet automatisme remplacera vos paramètres Away Mode. Sélectionnez les options que vous souhaitez configurer: Appuyez sur (F) et faites glisser la barre
Page 19 of 143