Showing 191 - 200 of 1,457 results

Page 20 of 146
  • Creating an automation

    LK FUGA® - Wiser wireless socket outlet 1½ M – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more information about , refer to the system user
  • Exxact - Connected Motion Sensor with Switch 10 A Wiser Home Device user guide

    single devicein the Wiser System. All functions will be accessible through the Homescreen. Away ModeAway Mode automatically turns off the Motion Sensor Switch. For example, whenyou are away from home for a long time, the light should not turn on due to falsemotion detections. This feature ensures the
  • System M and System D - Connected Thermostat 2 A, ZB Wiser Home Device user guide

    setpoint.Refer room settings, page 25 for more information on occupancy duration. When presence detect or setback has been activated, thermostat dot matrixdisplay shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° CCelsius and
  • System M and System D - Connected Thermostat 16 A, ZB Wiser Home Device user guide

    detect or setback has been activated, thermostat dot matrixdisplay shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° CCelsius and the inputs detect room occupancy, the thermostat will adhere to the23° C setpoint. However
  • Wiser Home System User Guide (Denmark)

    InsightHome Good evening Favourite devices Edit Motion SensorHallway Critical battery Unoccupied Moments Edit Away Mode Good night Tips and advice See all Stay safe and simulate your presencewith lights and shutters when you areaway for added security Show me Not for me ShutterLiving room Openuntil 16:00
  • Création d’un automatisme

    Climatiseur Airzone Plénum et Aidoo Pro – Guide de l'utilisateur de l’appareil Wiser Home

    appareil(E) qui définira la condition. Si vous avez sélectionné la condition comme Mode Absence et agir en tant que Contrôler un appareil alors cet automatisme remplacera vos paramètres Away Mode. Sélectionnez les options que vous souhaitez configurer: Appuyez sur (F) et faites glisser la barre
  • LK FUGA® Wiser wireless PIR with relay Wiser Home Device user guide

    device. NOTE: The Control tab will not be visible if you have only a single devicein the Wiser System. All functions will be accessible through the Homescreen. Away ModeAway Mode automatically turns off the Motion Sensor Switch. For example, whenyou are away from home for a long time, the light should
  • Creating an automation

    PowerTag Control – Device user guide

    based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): The Away Mode is intended to set your Home to a practical state for longer absences, such as leaving for the weekend. Maximum 10 conditions can be added. Select a
  • Wiser Plug Wiser Home Device User Guide

    any of the following (C): – Device status change: To select a device to enable automation.– Away Mode: Enable / Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information refer to Awaymode
  • System M and System D - Connected Thermostat 2 A, ZB

    Built in Automation Built in Automation There are three built in Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Boost All Boost All You can apply a boost of +2 °C
Page 20 of 146