Odace - Connected Thermostat 2 A – Wiser Home Device user guide
condition: This triggers an action when at least one condition is met. To add condition, tap Add conditions and select any of the following: Device status change (Select the device) Away Mode (Enable or Disable) Max. of 10 conditions can be added. To remove an added condition, swipe left and tap (D). To
-interconnected, and integrated PV systems. It is not suitable for any other application areas. RISK OF ELECTRIC SHOCK AND EQUIPMENT DAMAGE Keep inverter cables at least 30 mm away from any heat source. The use of inverter cables in a high temperature environment may cause aging and damage to the insulation
battery Unoccupied Moments Edit Away Mode Good night Tips and advice See all Stay safe and simulate your presencewith lights and shutters when you areaway for added security Show me Not for me ShutterLiving room Openuntil 16:00 Automations SUG_SV_FI_WH-02 57 Configuring the Wiser System 3. Tap Devices
amber on the device. Pairing not completed and returned to factorydefault. Pair the Wireless switch and the device again. Refer to• Relay switch, page 7 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless
zigbee signalstrength. Tap a Device in the List to navigate to the Device Details, page 64.1. Login to the app. 2. On the Home Screen, tap . Control InsightHome Good evening Favourite devices Edit Motion SensorHallway Critical battery Unoccupied Moments Edit Away Mode Good night Tips and advice See
List to navigate to the Device Details, page 79.1. Login to the app. 2. On the Home Screen, tap . Control InsightHome Good evening Favourite devices Edit Motion SensorHallway Critical battery Unoccupied Moments Edit Away Mode Good night Tips and advice See all Stay safe and simulate your presencewith
control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Push–button dimmer, page 8 The Wireless switch battery is discharged
Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide
is set in room settings. If there is no change in occupancy status during this period, the thermostat reverts to the unoccupied setpoint.Refer room settings for more information on occupancy duration. When presence detect or setback has been activated, thermostat dot matrix display shows away mode
Good evening Favourite devices Edit Motion SensorHallway Critical battery Unoccupied Moments Edit Away Mode Good night Tips and advice See all Stay safe and simulate your presencewith lights and shutters when you areaway for added security Show me Not for me ShutterLiving room Openuntil 16:00