Showing 211 - 220 of 327 results

Page 22 of 33
  • Exxact - Connected Relay Switch 10 A Wiser Home Device user guide

    reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Relay switch, page 7 The Wireless switch battery is discharged. Replace the battery of the Wireless
  • Wiser Micro Module Light Switch Wiser Home Device user guide

    . Refer to• Micro module light switch, page 9 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to
  • Wiser Micro Module Dimmer Wiser Home Device user guide

    opening of a shutter or thedetection of movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide.NOTE: Maximum 10 conditions can be added. a. In this
  • Advanced device settings

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    is set in room settings. If there is no change in occupancy status during this period, the thermostat reverts to the unoccupied setpoint.Refer room settings for more information on occupancy duration. When presence detect or setback has been activated, thermostat dot matrix display shows away mode
  • Unica - Connected Relay Switch 10 A Device user guide

    reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Relay switch, page 8 The Wireless switch battery is discharged. Replace the battery of the
  • Ovalis - Connected Universal Push-button Dimmer LED Device user guide

    Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Push–button dimmer, page 9 The Wireless switch battery is discharged. Replace the battery of the Wireless switch
  • Odace - Connected Universal Rotary Dimmer LED Device user guide

    Symptom Possible cause Solution LED displays amber on the device. Pairing not completed and returned to factorydefault. Pair the Wireless switch and the device again. Refer to• Rotary dimmer, page 8 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away
  • Wiser Boiler Relay Wiser Home Device user guide

    . B A 16 DUG_Boiler Relay_WH–05 Wiser Boiler Relay 4. Tap Add conditions and select any of the following (C):– Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights
  • Wiser Water Leakage Sensor Wiser Home Device user guide

    .– Away Mode: Enable / Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information about AwayMode, refer to the system user guide. e.g. Good Morning If When Conditions are met All conditions Any
  • Advanced device settings

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    is set in room settings. If there is no change in occupancy status during this period, the thermostat reverts to the unoccupied setpoint.Refer room settings for more information on occupancy duration. When presence detect or setback has been activated, thermostat dot matrix display shows away mode
Page 22 of 33