Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Push–button dimmer, page 9 The Wireless switch battery is discharged. Replace the battery of the Wireless
Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Push–button dimmer, page 9 The Wireless switch battery is discharged. Replace the battery of the Wireless switch
Symptom Possible cause Solution LED displays amber on the device. Pairing not completed and returned to factorydefault. Pair the Wireless switch and the device again. Refer to• Rotary dimmer, page 8 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away
: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information about AwayMode, refer to the system user guide. e.g. Good Morning If When
.– Any condition: This triggers an action when at least one condition is met. 4. Tap Add conditions and select any of the following (C):– Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger
the device. Pairing not completed and returned to factorydefault. Pair the Wireless switch and the device again. Refer to• Socket outlet, page 9 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a
any of the following (D):• Device status change: To select a device to enable automation.• Away Mode: To turn OFF the motion sensor and the device connected to it by enabling the this mode is enabled. When the away mode istriggered, sensitivity of the motion sensor turns OFF. TIP: You can enable the
the device. Pairing not completed and returned to factorydefault. Pair the Wireless switch and the device again. Refer to• Relay switch, page 7 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a
thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Socket outlet, page 7 The Wireless switch battery is discharged. Replace the battery of
and the device again. Refer to• Rotary dimmer, page 8 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer