Showing 251 - 260 of 328 results

Page 26 of 33
  • Wiser Home Essential API

    29 70 00 www.se.com Device Device The following topics are examples of fetching a list of devices, device details, and the away mode status. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Fetching the List of Devices Fetching the List of Devices
  • Sensor temperatura/humidade Wiser Guia de utilizador do dispositivo Wiser Home

    to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. SUGESTÃO: Away mode can also be used as a trigger to turn off thelights, dimmer or closing the shutter etc. For more information aboutAway Mode, refer to the system user guide. Se Quando Todas as Fechar Guardar B A P
  • Plenum Airzone e Aidoo Pro - Ar condicionado Wiser Home Guia de utilizador do dispositivo

    -iberic/English/System%20User%20Guide_Wiser_Home%20(Iberic)_DD00528175.xml/$/SUG_Home-Basics-Modes-Away-FDC909CB#SUG_Home-Basics-Modes-Away-FDC909CB2 https://www.productinfo.schneider-electric.com/wiser_home-dev2/wiser-home-sug-iberic/English/System%20User%20Guide_Wiser_Home%20(Iberic)_DD00528175.xml
  • Ovalis - Connected Blind Control Switch Device user guide

    switch not able to control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Blind control switches, page 7 The Wireless switch battery
  • PowerTag Control Device user guide

    device status, such as the opening of a shutter or thedetection of movement by a motion sensor. – Away Mode (Enable or Disable): The Away Mode is intended to set yourHome to a practical state for longer absences, such as leaving for theweekend.NOTE: Maximum 10 conditions can be added. 5. Select a device
  • Odace - Connected Blind Control Switch Wiser Home Device user guide

    are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Blind control switches, page 8 The Wireless switch battery is discharged. Replace the battery of the Wireless switch Scenario Procedure
  • Wiser Micromodule for Fil Pilote radiators Device user guide

    )– Away Mode (Enable or Disable) NOTE: Maximum 10 conditions can be added. 5. Select a device (E) that will set the condition and then select Set point (F). New automation If When Conditions are met All conditions Start by adding a condition that willtrigger your automation Any condition 0 of 10 Then
  • Schneider Charge Device user guide

    you are away. NOTE: EV Charger can only act as an action. 1. On the Home page, tap . 2. Go to Automation and then tap to create an automation. 3. Tap and choose an icon that best represents your automation. 4. Enter a name of the automation (A) and select any of the following conditionsto meet (B
  • Sensor de Temperatura/Humedad Wiser Manual del usuario del dispositivo Wiser Home

    when all conditions are met.– Any condition: This triggers an action when at least one condition is met. 4. Tap Add conditions and select any of the following (C):– Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. SUGERENCIA: Away
  • Wiser Plug

    of an automation In the example below, if away mode is enabled during Daytime, then Plug will turn off. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Editing an automation Editing an automation Schneider Electric 35 rue
Page 26 of 33