Showing 291 - 300 of 1,457 results

Page 30 of 146
  • Wiser Temperature/Humidity Sensor Wiser Home Device user guide

    conditions are met.– Any condition: This triggers an action when at least one condition is met. 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be
  • Oprettelse af en automatisering

    Wiser trådløs jalousi styring for indbygning (puck) – Brugervejledning til Wiser Home-enheden

    kun en handling, når alle betingelser er opfyldt. Enhver tilstand: Dette udløser en handling, når mindst én betingelse er opfyldt. Tryk på Tilføj betingelser, og vælg en af følgende (C): Ændring af enhedens status: Vælg en enhed for at aktivere automatisering. Væk-tilstand: Aktivér / Deaktiver away
  • Ovalis - Connected Blind Control Switch Wiser Home Device user guide

    motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. For more informationabout Away Mode, refer to the system user guide. NOTE: Maximum 10 conditions can be added. a. In this example, we will select Device status change and
  • Unica - Connected Blind Control Switch Wiser Home Device user guide

    automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. For more informationabout Away Mode, refer to the
  • Exxact - Connected Blind Control Switch Wiser Home Device user guide

    (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. For more
  • Wiser Room Thermostat Wiser Home Device user guide

    conditions Start by adding a condition that will triggeryour automation. B A 26 DUG_Room Thermostat_WH-09 Wiser Room Thermostat 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an
  • Unica - Connected Universal Push-button Dimmer LED Wiser Home Device User Guide

    automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. Refer to the AwayMode topic in the respective
  • Ovalis - Connected Relay Switch 10 A Wiser Home Device user guide

    any of the following (C): – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On the
  • Unica - Connected Relay Switch 10 A Wiser Home Device user guide

    opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. NOTE: Maximum 10 conditions can be added. a. In
  • Odace - Connected Relay Switch 10 A Wiser Home Device user guide

    detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. NOTE: Maximum 10 conditions can be added. a. In this example, we will select
Page 30 of 146