Showing 301 - 310 of 1,457 results

Page 31 of 146
  • Exxact - Connected Motion Sensor with Switch 10 A

    Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider
  • Exxact - Connected Motion Sensor with Multiwire Dimmer

    ) 1 41 29 70 00 www.se.com Adjusting the brightness level using app Adjusting the brightness level using app Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France
  • LK FUGA® Wiser wireless PIR with relay

    www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison
  • Odace - Connected Relay Switch 10 A Wiser Home Device user guide

    detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. NOTE: Maximum 10 conditions can be added. a. In this example, we will select
  • Exxact - Connected Relay Switch 10 A Wiser Home Device user guide

    (B) and select any of the following (C): – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to
  • Exxact - Connected Multiwire Universal Push-button Dimmer LED Wiser Home Device user guide

    triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide
  • Wiser Micro Module Light Switch Wiser Home Device user guide

    , such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. NOTE: Maximum 10 conditions can be
  • EVlink Home Smart Wiser Home device user guide

    to trigger an automation. 5. Tap Add conditions (C) and select any of the following (D): – Device status change (Select the device)– Away Mode (Enable or Disable)– Energy Price changes (To define the energy price limit.) NOTE: This condition is available only if your tariff is set to Peak/Off-Peak
  • Unica - Connected Universal Rotary Dimmer LED Wiser Home Device User Guide

    . – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. NOTE: Maximum 10 conditions can be added. a. In this example, we will select Device status change and choose adevice to
  • Exxact - Connected Multiwire Universal Rotary Dimmer LED Wiser Home Device user guide

    will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User
Page 31 of 146