Showing 3,261 - 3,270 of 9,859 results

Page 327 of 986
  • Termostato Radiador Wiser

    Malmaison França + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric CCTFR6100 CCTFR6101 CCTFR6100Z3 Acerca do dispositivo Acerca do dispositivo O Termostato Radiador Wiser (a seguir designado Termóstato) utiliza sensores de temperatura integrados para controlar o fluxo de água através de um radiador
  • Funcionamiento del interruptor de relé

    Sistema M y sistema D - Interruptor inalámbrico de una/dos teclas conectado – Guía del usuario del dispositivo Wiser Home

  • Boost All

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Boost All Boost All Boost All You can apply a +2 °C boost for 1 hour to all rooms in the system. This action does not affect hot water. Since it is a one-time action, you will find Boost All (A) under the Automation menu by tapping the Automations tab at the bottom of the Home screen.
  • EcoWatt User Guide

    . This document is not intended as a substitute for a detailed study or operational andsite-specific development or schematic plan. It is not to be used for determiningsuitability or reliability of the products/solutions for specific user applications. It is theduty of any such user to perform or have
  • Enchufe inalámbrico Guía del usuario del dispositivo Wiser Home

    documento contiene descripciones generales,características técnicas o recomendaciones relacionadas con productos osoluciones. Este documento no pretende sustituir a un estudio detallado o un plan de desarrollo oesquemático específico de operaciones o sitios. No debe usarse para determinar laadecuación o la
  • Google Home

    Termostato de habitación Wiser – Guía del usuario del dispositivo Wiser Home

    Google Home Google Home Google Home Google Home es una marca de altavoces inteligentes que funcionan de manera similar a Amazon Alexa. El usuario puede hablar con una profusión de comandos para solicitar información o pedir a Asistente de Google que realice una acción. Comandos comunes de Wiser
  • Safety Information

    Unica - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure. The addition of either symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are
  • Safety Information

    Ovalis - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure. The addition of either symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are
  • Safety Information

    Unica - Connected Relay Switch 10 A – Wiser Home Device user guide

    or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure. The addition of either symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are
  • Definir as definições lux

    Unica - Detetor de movimento variador LED conectável – Guia do utilizador do dispositivo Wiser Home

    Definir as definições lux Definir as definições lux Definir as definições lux Pode definir o valor limite para intervalos de lux (como muito escuro, escuro, claro e muito claro) do ambiente. Isto evitará a deteção falsa causada por alterações na intensidade da luz. No ecrã Inicial, toque em . Toque
Page 327 of 986