Showing 371 - 380 of 1,648 results

Page 38 of 165
  • Setting the detection sensitivity

    Exxact - Connected Motion Sensor with Push-button Dimmer LED – Wiser Home Device user guide

    Setting the detection sensitivity Setting the detection sensitivity Setting the detection sensitivity You can set the sensitivity level of the sensor. On the Home screen, tap . Tap Devices Lights Motion Dimmer Motion Detection Sensitivity and select any one of the following options: Low: Detects
  • Setting the device location

    LK FUGA® Wiser wireless PIR with relay – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting the device location

    LK FUGA® Wiser wireless PIR dimmer with neutral – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting up a schedule

    LK FUGA® Wiser wireless PIR dimmer with neutral – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The Motion Sensor Dimmer can be fully controlled by a schedule. Once the schedule is set, the Motion Sensor Dimmer operates at a given time. On the Home screen, tap . Go to Schedules and tap to create a schedule. Enter the name of
  • Setting up a schedule

    LK FUGA® Wiser wireless double relay – Wiser Home Device User Guide

    Setting up a schedule Setting up a schedule Setting up a schedule The relay switch can be fully controlled by a schedule. Once the schedule is set, the relay switch operates at a given time. On the Home screen, tap . Go to Schedules and tap to create a schedule. Enter the name of the schedule (A
  • Setting the device location

    LK FUGA® Wiser wireless double relay – Wiser Home Device User Guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting the device location

    Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location Using the Wiser Home app, you can assign the Relay in the room (such as bedroom, living room, dining room etc.). To assign the Relay location: On the Home screen, tap . Tap Devices Climate 16A Relay Location (A) to assign the Relay to the existing room or a new room (B) and tap Submit. You can configure up to 4 Relays in the same room.
  • Setting the device location

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting the configure duration

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    Setting the configure duration Setting the configure duration Setting the configure duration Each shutter motor varies in the time it takes to complete the opening/closing movement (i.e., edge to edge). Therefore, the opening/closing time of the shutter must be determined in the app. To determine
  • Setting the room temperature

    Wiser Room Thermostat – Wiser Home Device user guide

    Setting the room temperature Setting the room temperature Setting the room temperature You can set the room temperature manually using the room thermostat button or remotely using the Wiser Home app.
Page 38 of 165