Showing 4,711 - 4,720 of 9,846 results

Page 472 of 985
  • Configuring - feed in tariff

    Wiser Home – System User Guide (Denmark)

    Insights page, tap Find out more and read the Feed-in Tariff onboarding information. Tap to close the overlay screen. If you have not configured your Feed-in tariff, a push notification will be sent after 2 weeks and the last reminder after 6 weeks. If you have closed the reminder splash screen, you can
  • Configuring - feed in tariff

    Wiser Home – System User Guide (UK, Ireland)

    Insights page, tap Find out more and read the Feed-in Tariff onboarding information. Tap to close the overlay screen. If you have not configured your Feed-in tariff, a push notification will be sent after 2 weeks and the last reminder after 6 weeks. If you have closed the reminder splash screen, you can
  • Anti-Tripping Management

    Exxact - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    algorithm designed to prevent global overconsumption. It achieves this by reducing setpoints and shutting down specific loads, ensuring that overall energy consumption stays within a predefined limit. With the integration of Wiser Home, users gain enhanced control over the loads monitored by the
  • Micromódulo Variador Wiser

    ) 1 41 29 70 00 www.se.com Schneider Electric Acerca do dispositivo Acerca do dispositivo O micromódulo variador Wiser (a seguir designado por dispositivo) combina as vantagens de funcionalidade de um variador inteligente com os interruptores de botão de pressão mecânicos comuns. Transforma um
  • Micromódulo variador multifios

    Unica - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    ligado ao botão de pressão mecânico direito. Remova o botão basculante do interruptor sem fios. Prima brevemente o botão de pressão superior do lado direito 5 vezes numa sequência rápida no interruptor sem fios. O LED de estado pisca a verde. PERIGO DE CHOQUE ELÉTRICO Cumpra os regulamentos ao
  • Troubleshooting in Quick Home Connect

    Unica - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    outlet Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Socket outlet The Wireless switch
  • Troubleshooting in Quick Home Connect

    Ovalis - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    outlet Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Socket outlet The Wireless switch
  • Troubleshooting in Quick Home Connect

    Odace - Connected Relay Switch 10 A – Wiser Home Device user guide

    switch Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Relay switch The Wireless switch battery
  • Troubleshooting

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    Unable to set the room temperature by the app. Wiser Hub signal is weak or not connected to the Wi-Fi ® network. Check for a Wi-Fi ® signal. Find and Bind When the user press and holds the rotary push-button for >8s, "Fb" LED is displayed on the thermostat matrix display.It is a Zigbee function, can be ignored. “X” mark is displayed on LED matrix Device is lock and LED matrix displays “X” Press rotary push-button for > 5 s to exit the menu.
  • eSetup App

    Wiser Home – System User Guide (Spain and Portugal)

    . This dedicated application for Electricians is a commissioning tool for Wiser devices in residential and SmartLink, Powertag devices in Small Buildings. Not all the wiser devices can be configured using the eSetup app. The app offer the configuration for devices such as Light and Shutter Devices
Page 472 of 985