Showing 501 - 510 of 1,241 results

Page 51 of 125
  • Remover o dispositivo do sistema Wiser

    EVlink Home Smart – Manual do utilizador do dispositivo doméstico Wiser

    Remover o dispositivo do sistema Wiser Remover o dispositivo do sistema Wiser Remover o dispositivo do sistema Wiser Através da aplicação Wiser Home, pode remover o dispositivo da lista de dispositivos. No separador Controlo, toque em Todos EVlink Home Smart Definições do dispositivo. Toque em
  • Eliminación del dispositivo del sistema Wiser

    EVlink Home Smart – Manual del usuario del dispositivo Wiser Home

    Eliminación del dispositivo del sistema Wiser Eliminación del dispositivo del sistema Wiser Eliminación del dispositivo del sistema Wiser Con la aplicación Wiser Home puede eliminar un dispositivo de la lista de dispositivos. En la pestaña Control, toque Todo EVLink Home Smart Ajustes del
  • Setting boost mode manually

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    Setting boost mode manually Setting boost mode manually Setting boost mode manually You can enable and disable boost mode manually.When enabled the temperature increases by 2° C for temperature control modes and by +2 over the setpoint. To enable boost mode: Press the rotary push-button until the
  • Réglage du niveau de lux

    Capteur de mouvement extérieur ARGUS 360 – Guide de l'utilisateur de l’appareil Wiser Home

    détecté, les dispositifs associés au capteur de mouvement sont activés. Pour régler le niveau de lux : Sur l’écran Détails de l’appareil, appuyez sur Niveau de Lux. Sélectionnez l'un des modes suivants : Mode Jour : Pour les dispositifs devant être actifs de jour et de nuit. Le dispositif fonctionne
  • Setting the motion detection timer

    ARGUS Motion Sensor Outdoor 360 – Wiser Home Device user guide

    . Select one of the following modes: Test Mode: To test the motion sensor and make sure that its placement and detection range are as required. In this mode, the device connected to the motion sensor turns ON for 2 seconds after motion detection and then goes OFF for 3 seconds. If the motion is still
  • Tariff

    Wiser Smart Plug 16A – Wiser Home Device User Guide

  • Google Home

    Wiser Home – System User Guide (Spain and Portugal)

    Google Home Google Home Google Home Google Home is a brand of smart speakers that work similarly to Amazon Echo. Google’s intelligent PA, Google Assistant, is equivalent to Amazon’s Alexa. Google Home is also available on all Android devices and does not require the use of the ‘Smart Speakers’. The
  • Het apparaat installeren

    PowerTag Energy – Wiser Home Gebruikershandleiding voor het apparaat

    ) PowerTag Acti9 F63 (nl, ro, ru, zh) Installatievideo: Installatie PowerTag E Ondersteunde montageposities Ondersteunde montageposities Ondersteunde montageposities Resi9 Montagepositie Smart Tag Modelnummer Boven- of onderzijde PowerTag-energie R9 M63 1PW R9M20 Boven- of onderzijde PowerTag-energie R9
  • Installieren des Geräts

    PowerTag – Wiser Home Geräte-Benutzerhandbuch

    , pt) PowerTag Acti9 F63 (nl, ro, ru, zh) Installationsvideo: PowerTag E-Installation Unterstützte Einbaupositionen Unterstützte Einbaupositionen Unterstützte Einbaupositionen Resi9 Einbauposition Smart Tag Modellnummer Obere Schalterfläche oder untere Schalterfläche PowerTag R9 M63 1PW R9M20 Obere
  • Einen Moment löschen

    Wiser Smart Plug 16A – Wiser Home Geräte-Benutzerhandbuch

Page 51 of 125