Showing 571 - 580 of 1,457 results

Page 58 of 146
  • Wiser Smoke Alarm - Battery Wiser Home Device user guide

    within anautomation. NOTE: To remove an action, swipe left on the action and tap (G). Add an action Please choose an action for yourautomation. Control a deviceE.g. turn the light on E.g. if the motion is detected Activate a momentE.g. enable Away mode WaitE.g. wait 10 mins until next action F e.g. Good
  • Affichage LED

    Unica - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    Affichage LED Affichage LED Affichage LED Appairage Action de l’utilisateur Affichage de la LED État Appuyez 3 fois sur le bouton-poussoir La LED clignote en orange une fois par seconde. Le mode d’appairage est actif pendant 30 secondes. Une fois l’appairage terminé, la LED s’allume en vert pendant
  • Setting the lux level

    ARGUS Motion Sensor Outdoor 360 – Wiser Home Device user guide

    . To adjust the lux level: On the Device Details screen, tap Lux level. Select one of the following modes: Day Mode: For the devices which should be active during the days and the nights. The device operates irrespective of any lux value. Night Mode: For the devices which should be active in low light
  • Troubleshooting

    Unica - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    . Reduce load. Change load. Check wiring between the push button and the Dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Troubleshooting

    LK FUGA® Wiser wireless dimmer – Wiser Home Device User Guide

    overheating. Reduce load. Change load. Check wiring between the push button and the dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Selecionar o modo de funcionamento

    Sensor porta/janela Wiser – Guia do utilizador do dispositivo Wiser Home

  • Climate control

    Wiser Home – System User Guide (Spain and Portugal)

    system is in cooling mode in a non-cooling room: The Radiator Thermostat shall not perform a Boost and shall display the same status as in Device Lock mode. The Room thermostat shall wake up using any of the 3 keys (+, -, O), but subsequent button presses will not change the set point. Domestic
  • Affichages LED

    PowerTag Energy – Guide de l’utilisateur de l’appareil Wiser Home

    Affichages LED Affichages LED Affichages LED Comportement Voyant de communication PowerTag éteint. Le PowerTag recherche une passerelle en mode d’appairage. Le PowerTag est en mode d’identification. Le PowerTag est en réseau. Communication normale avec la passerelle. Perte de communication occasionnelle. Perte de communication avec la passerelle. Erreur interne détectée.
  • LED indications

    PowerTag Energy – Wiser Home Device user guide

    LED indications LED indications LED indications Behavior Communication indicator light PowerTag switched off. PowerTag is searching for a Hub in pairing mode. PowerTag is in identification mode. PowerTag is in network. Normal communication with the Hub. Occasional loss of communication. Loss of communication with the Hub. Internal error detected.
  • Wiser Tête de Vanne Thermostatique

    Automatismes intégrés Automatismes intégrés Trois automates sont intégrés, tels que Boost All, Cancel all overrides et Away mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil-Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Tout booster Tout booster Vous pouvez booster la
Page 58 of 146