Showing 731 - 740 of 1,241 results

Page 74 of 125
  • Personliggjorte energiindsigter (anslået energi)

    PowerTag Energy – Wiser Home Brugervejledning til enheden

    øverst, er baseret på brugen i hele området. Hvis Evlink home Smart f.eks. ikke bruges så meget i oktober, vises det på kortet Andre (D). Den opdaterede forbrugsværdi vises i fordelingsdelen, når du ruller ned. De brugerdefinerede etiketter for belastninger er grupperet i fordelingen Andre (D). Indsigter
  • Fehlerbehebung

    System M und System D - Connected Raumtemperaturregler 16 A, ZB – Wiser Home Geräte-Benutzerhandbuch

    Wiser Hub näher an den Thermostat. Erweitern Sie die Bereich mit dem Wiser Smart Plug. Verbindung zum Wiser Hub nicht möglich (rote LED blinkt) Schlechtes Signal zwischen Wiser Hub und Thermostat. Die Geräte verfügen über keine Spannung (Thermostat/ Wiser Hub/Wi-Fi ®-Netzwerk). Verbinden Sie den
  • Eco Mode

    Wiser Home – System User Guide (Sweden, Finland)

    Eco Mode Eco Mode Eco Mode Eco Mode is a smart feature designed to maximize the efficiency of your heating system. It automatically optimizes the stop time of the heating phase, each time the set temperature changes from a higher to lower value. Eco Mode is a system feature that is either activated
  • Limitations of the Wiser System

    Wiser Home – System User Guide (Denmark)

    overall Maximum per Room Shutter Devices 32 32 Appliances Maximum overall Maximum per Room Any combination of the following ON/OFF appliances Connected Sockets Smart Plugs Wiser Power Micromodule 20 20 LK FUGA ® Wiser Wireless Battery 4 Button Switch 10 10 Safety and Security Maximum overall Maximum per
  • Stemmestyring

    Wiser Smat Plug 16 A – Brugervejledning til Wiser Home-enheden

  • Creating an automation

    Unica - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    actions within an automation. In this example, we will initially select Control a device and select Smart Socket (F) as the device to trigger an action, later, we will select for the Wait option to add a delay in the automation. You cannot select the same device that you selected for Add conditions in
  • Energy

    Wiser Home – System User Guide (Germany, Austria)

    PowerTag C A9XMC1D3 Control and monitoring wireless communication module Instruction Sheet Device User Guide EVlink Home Smart EVH4xxxN EVH4xxxNC Supplies electric energy to charge plug-in electric vehicles Instruction Sheet Device User Guide Schneider Charge EVH5A22N2S EVH5A11N2CX EVH5A07N2CX
  • Konfiguration af enheden

    Wiser Smat Plug 16 A – Brugervejledning til Wiser Home-enheden

  • Creating an automation

    Wiser Smart Plug 16A – Wiser Home Device User Guide

    wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation. Tap Control a device > Smart Plug, tap (F) to turn on/off, then tap Set. Maximum 10 actions can be added. To remove an action, swipe left on the action
Page 74 of 125