Showing 801 - 810 of 1,622 results

Page 81 of 163
  • Insights

    Wiser Home – System User Guide (Denmark)

    timeframe (days, months and years). B Shows the percentage of energy saved for the current month, along with a 3-month average comparison. It also provides data on hours saved in Away Mode and allows you to enable Eco Mode for additional savings. C Tracks adjustments made to heating, including the
  • About Aidoo Pro Wi-Fi® and Wiser System

    Airzone - Aidoo Pro Heat Pump – Wiser Home Device user guide

    the current temperature, set point, and status of each heating zone. Comprehensive Control: Manage home heating by creating, editing, and managing schedules and modes such as Eco, Comfort, and Away. Hot Water Management: Easily create schedules and boost domestic hot water using the Wiser Home app
  • Creating a moment

    Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • Creating a moment

    Wiser Radiator Thermostat – Wiser Home Device user guide

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • Creating a moment

    Wiser Underfloor Heating Controller / Connection Strip – Wiser Home Device user guide

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • Creating a moment

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • Creating a moment

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • Using the device

    Schneider Charge – Wiser Home Device user guide

    E, F, G, H, J. A Total cost of charging session. B Total time of charging in the session. C Total energy consumption in the session. D Control button (Start charging/Stop charging, Pause/Resume). E To select the charging mode. Refer to Charging Mode. F To see the 24 hr schedule based on the
  • Adding a Device

    Wiser Home – System User Guide (France)

    the Device into pairing mode. The Wiser Home App will guide you through the pairing process. You can find detailed information about the pairing mode in the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices. When the
  • Adding a Device

    Wiser Home – System User Guide (Germany, Austria)

    Home Smart PowerTag Energy Schneider Charge Wiser Plug Wiser Radiator Thermostat Wiser Room Thermostat Wiser Underfloor Heating Controller / Connection Strip If you are facing difficulties in scanning the QR code, refer to Handling QR code Issues. Tap Next. Set the Device into pairing mode. The
Page 81 of 163