Showing 8,431 - 8,440 of 9,888 results

Page 844 of 989
  • Turning On/Off device using app

    Ovalis - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    Turning On/Off device using app Turning On/Off device using app Turning On/Off device using app On the Control tab, tap All devices or the room tab where the dimmer is located. Tap (A) to turn on/off dimmer. You can also turn the device on/off and adjust the brightness from the Home screen when you add it to your Favourite.
  • Volet avec lames inclinables

    Ovalis - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    Volet avec lames inclinables Volet avec lames inclinables Volet avec lames inclinables Sur l’écran d’accueil, appuyez sur . Appuyez sur Equipements Volets Volet avec lames inclinables. Appuyez sur Durée d’ouverture/ Durée de fermeture (A) et saisissez la durée d’ouverture/fermeture du volet
  • Connecting Devices to the Hub

    Wiser Home – System User Guide (Germany, Austria)

    Connecting Devices to the Hub Connecting Devices to the Hub Connecting Devices to the Hub For the Wiser devices to be controlled by the hub, they must be connected to the hub. Connecting devices to the hub is part of the set up process. You can add devices to the hub at any time. The app guides you through the process of adding devices. You can find detailed information about the necessary steps for adding the device in the chapter Adding a Device.
  • Utilizar o dispositivo

    Sensor temperatura/humidade Wiser – Guia do utilizador do dispositivo Wiser Home

    controlo do sensor, pode ver o seguinte: O valor da temperatura atual (A) O valor da humidade atual (B) Histórico (C) Definições do dispositivo (D) Adicionar aos favoritos (E)
  • Utilizar o dispositivo

    Sensor fuga de água Wiser – Guia do utilizador do dispositivo Wiser Home

    Utilizar o dispositivo Utilizar o dispositivo Utilizar o dispositivo O Painel de Controlo do sensor permite-lhe monitorizar o estado atual da deteção de fuga de água. No separador Controlo, toque em Todos os dispositivos ou num separador da divisão onde está o sensor Na página do painel de controlo do sensor, pode ver o seguinte: Estado de fuga de água (A) Histórico (B) Definições do dispositivo (C) Adicionar aos favoritos (D)
  • Activer/désactiver l’appareil à l’aide de l’application

    Unica - Interrupteur variateur universel LED connecté – Guide de l'utilisateur de l'appareil Wiser Home

    Activer/désactiver l’appareil à l’aide de l’application Activer/désactiver l’appareil à l’aide de l’application Activer/désactiver l’appareil à l’aide de l’application Dans l’onglet Contrôle, appuyez sur Tous les appareils ou sur l’onglet de la pièce où se trouve le variateur. Appuyez sur (A) pour
  • Resetting the device

    Unica - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    stops blinking upon successful reset of the device. The Push-button Dimmer restarts and blinks green for a few seconds. After reset, the LED turns amber indicating that it is ready for pairing.
  • Turning On/Off device using app

    Unica - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    Turning On/Off device using app Turning On/Off device using app Turning On/Off device using app On the Control tab, tap All devices or the room tab where the dimmer is located. Tap (A) to turn on/off dimmer. You can also turn the device on/off and adjust the brightness from the Home screen when you add it to your Favourite.
  • Activer/désactiver l’appareil à l’aide de l’application

    Unica - Variateur rotatif universel connecté – Guide de l'utilisateur de l'appareil domestique Wiser

    Activer/désactiver l’appareil à l’aide de l’application Activer/désactiver l’appareil à l’aide de l’application Activer/désactiver l’appareil à l’aide de l’application Dans l’onglet Contrôle, appuyez sur Tous les appareils ou sur l’onglet de la pièce où se trouve le variateur. Appuyez sur (A) pour
  • Activer/désactiver l’appareil à l’aide de l’application

    Odace - Interrupteur variateur universel LED connecté – Guide de l'utilisateur de l’appareil Wiser Home

    Activer/désactiver l’appareil à l’aide de l’application Activer/désactiver l’appareil à l’aide de l’application Activer/désactiver l’appareil à l’aide de l’application Dans l’onglet Contrôle, appuyez sur Tous les appareils ou sur l’onglet de la pièce où se trouve le variateur. Appuyez sur (A) pour
Page 844 of 989