Showing 861 - 870 of 1,449 results

Page 87 of 145
  • LED Indications in Quick Home Connect

    LK One Wiser Push-button Switch – Wiser Home Device user guide

    LED Indications in Quick Home Connect LED Indications in Quick Home Connect LED Indications in Quick Home Connect Pairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quick succession. LED blinks green, once per second. Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.
  • LED Indications in Quick Home Connect

    LK FUGA Wiser Multiwire LED Push-button Dimmer – Wiser Home Device user guide

    LED Indications in Quick Home Connect LED Indications in Quick Home Connect LED Indications in Quick Home Connect Pairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quick succession. LED blinks green, once per second. Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.
  • Resetting the device

    Wiser Power Micromodule – Wiser Home Device User Guide

    Resetting the device Resetting the device Resetting the device Select any one of the options to reset the device to factory default mode based on your installation: Short press the mechanical push-button 3 times and then long press once (>10 s). Short press the Setup/Reset button of the module 3 times and then long press once (>10 s) on the module.
  • Resetting the device manually

    Wiser Smoke Alarm - Battery – Wiser Home Device user guide

    Resetting the device manually Resetting the device manually Resetting the device manually Short press (< 0,5 s) the Setup/Reset button 3 times and then long press the Setup/Reset button once for >10 s to reset the smoke alarm to factory default mode. All configuration data, user data and network data are deleted.
  • Création d’un moment

    Wiser Actionneur de Chauffage électrique pour la commande de température – Guide de l’utilisateur de l’appareil

    placez le curseur (D) au bas de la barre pour le moment, le mode Protection contre le gel est activé. En mode Protection contre le gel, le système maintient la température dans la pièce à 5 °C. Lorsque la condition souhaitée est définie, appuyez sur Enregistrer. Une fois toutes les conditions
  • Creating a Schedule/Event

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    schedule, the Frost Protection mode is activated when the schedule begins.In the frost protection mode, the system maintains the room temperature at 5 °C. Set time (for example 12:00). A maximum of 8 events can be created per day. You can tap to copy the schedule from one day to other days or copy the
  • Creating a Schedule/Event

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    schedule, the Frost Protection mode is activated when the schedule begins.In the frost protection mode, the system maintains the room temperature at 5 °C. Set time (for example 12:00). A maximum of 8 events can be created per day. You can tap to copy the schedule from one day to other days or copy the
  • Setting the threshold temperature

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    Setting the threshold temperature Setting the threshold temperature Setting the threshold temperature Using the Wiser Home app, you can define the inside and outside temperature of a room above which the shutters shall close. To set the threshold inside and outside temperature: In the Seasonal Comfort Mode set-up page, tap Temperature. Set the inside and outside desired temperatures and tap Set.
  • Création d’un automatisme

    Wiser micromodule pour variateur – Guide de l'utilisateur de l’appareil Wiser Home

    . Mode Absence (activez ou désactivez) : Le mode Absence peut également déclencher un automatisme pour allumer les lumières, fermer les volets, etc. Reportez-vous à la rubrique Mode Absence dans le Guide de l’utilisateur du système correspondant. Vous pouvez ajouter jusqu’à 10 conditions. Dans cet
  • Création d’un automatisme

    Ovalis - Interrupteur à relais 10A connecté – Guide de l'utilisateur du dispositif Wiser Home

    Ajouter des conditions (B) et sélectionnez l’une des options suivantes (C) : Changement d’état d’un équipement (sélectionnez l’appareil) : Un automatisme est déclenché en fonction de l’état d’un appareil, tel que l’ouverture d’un volet ou la détection d’un mouvement par un capteur de mouvement. Mode
Page 87 of 145