DUG_SysM/SysD SSO_WH-05

Pairing the device

Using the Wiser Home app, pair your Socket outlet with the Wiser Hub to access and control the Socket outlet.
To pair the Socket outlet:
  1. On the Home page, tap .
  2. Tap Devices > and tap Appliances > Connected Socket > Next.
    TIP: The next screen shows the joining process of Socket outlet.
  3. Short press the push button 3 times on the Socket outlet.
    Make sure the LED blinks amber.
  4. Wait for a few seconds until the LED turns green. You can also see in the app that the Socket outlet is joined.

  5. Once the device is joined, tap (A) and select an icon suitable for your load and tap Save.
    NOTE: Electric plug icon is assigned by default.
  6. Tap (B) and assign a name.
  7. Tap Next to assign the Socket outlet to an existing room or a new room.
  8. Tap Submit.
You can see the added Socket outlet on the Home page under the room tab or under ALL devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?