DUG_Push-button Module, 1-gang/2-gang_WH-02

Shutter calibration

The shutter motor is supplied in an uncalibrated state. Each shutter motor varies in the time it takes to complete the opening/closing movement (i.e., edge to edge).

IMPORTANT:
  • It is necessary to select the device type and set the default run time before proceeding with shutter calibration. Refer to Refer to Selecting device type and Setting default run time.

  • Do not use the shutter either manually or on the app during calibration to avoid interruption.

  • Follow the procedure for shutter calibration according to the device type: Shutter or Shutter with tilting slats.

Shutter

  1. Upon setting the default run time, go to the Home page, tap All and find the device.

  2. On the control panel page, drag the sliding bar up/down to set the desired shutter opening percentage (A).

    The shutter opens completely and then it reaches to the desired position set in step 2. The shutter is now calibrated.

Shutter with tilting slats

  1. On the Home page, tap All and find the device.

  2. On the control panel page, in the Position tab, drag the sliding bar up/down to set the desired shutter opening percentage (A).

  3. Tap Slat Tilt

    tab, drag the sliding bar up/down to set the desired shutter opening percentage (B) according to any one of the following tilt position:
    • Horizontal

    • Tilted

    • Vertical

QR code for this page

Was this helpful?