DUG_Push-button Module, 1-gang/2-gang_WH-02

Identifying the device

Using the Wiser Home app, you can identify a 1-gang switch from the other available devices in the room.
To identify the 1-gang switch:
  1. On the Home page, tap .
  2. Tap Devices > 1-gang Switch > Identify (A).
    NOTE:
    • This feature flashes the 1-gang switch LED, so you can identify the actual device. It also switches connected loads on/off.

    • The 1-gang switch LED will continue to flash until you tap OK.

QR code for this page

Was this helpful?