DUG_Push-button Module, 1-gang/2-gang_WH-02

Troubleshooting

Symptom

Solution

Switch  

The device is not ready to pair after the device is removed from the app

Reset to factory default settings.

   
Dimmer  

Dimming up not possible

  • Reduce or increase load

  • Allow the pushbutton to cool in case of overheating

  • Change the load (if the load is incompatibe with the dimmer)

Switching on not possible

  • Allow the pushbutton to cool in case of overheating

  • Reduce load

  • Change load

  • Check wiring

Flickering at minimum brightness

  • Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device)

  • Change the load (if the minimum brightness is insufficient)

  • Set RL LED mode (it is advised to use 10% of nominal load to avoid overheating of the dimmer)

Flickering

  • Change load

  • Set RL LED mode (it is advised to use 10% of nominal load to avoid overheating of the dimmer)

Only slight dimming capability

  • Change dimming range

  • Set RL LED mode (it is advised to use 10% of nominal load to avoid overheating of the dimmer)

  • Change the load (if the load is incompatible with the dimmer)

   
Shutter  

No shutter movement or uncontrolled shutter movement

  • Check power supply

  • Change the load

  • Change wiring

Symptom

Possible cause

Solution

The device is not able to connect with the Hub. After pressing 3 times, the device LED blinks green/red for 30 s.

NOTE: This does not apply to newer Zigbee®
model.

Pairing mode has changed.

  1. Factory reset the device.
  2. After reset, press top right corner of the switch for 4 times and then hold for 20 s, until the LED blinks red.

    The device should reboot into the correct mode.

  3. After reboot, press 3 times on top right corner of the switch to initiate pairing mode.

    LED flashes orange.

QR code for this page

Was this helpful?