About the device
The Push-button module can be completed with:
-
corresponding 1-gang or 2-gang rockers
-
Frame in the corresponding design
-
corresponding inserts for switch, dimmer, and shutter or blind control
Switch insert Dimmer insert Shutter insert Blind control insert
Features of a push-button module
-
The Push-button module supports functionality such as switching, dimming and shutter control.
-
With the Wiser app, you can combine the settings of one or more devices to form a Moment or an Automation.
-
You can create a schedule for the various device functions in an easy manner as per your specific requirements for comfort and convenience.
1-gang switch, combination of:
Control options
Home control using Wiser Home app: To control the push button module through the Wiser app you will need the . Refer to .
Direct operation: The blind control switch can always be controlled directly on-site. You can also connect it with mechanical double push-buttons. Refer to Manual operation.