DUG_Push-button Module, 1-gang/2-gang_WH-02

Setting minimum or maximum brightness

Using the Wiser Home app, you can set minimum or maximum brightness.
To set minimum or maximum brightness:
  1. On the Home page, tap .
  2. Tap Devices > 1-gang Dimmer and use the slider control (A) to set minimum or maximum brightness.
    TIP: You can enable RL-LED Mode (B) if the 1-gang dimmer is connected to an LED lamp. It is recommended using this mode when you experience flickering of the bulb. Verify the lamp manufacturer’s specifications and the reduced power of the dimmer.
    NOTE: The Min/Max brightness settings and RL-LED mode features are not for 2-Gang Dimmer.

QR code for this page

Was this helpful?