DUG_Push-button Module, 1-gang/2-gang_WH-02

Resetting the device

You can reset the pushbutton to the factory default. It can be reset manually at any time, e.g., when the Hub is replaced.

Short press the top-center pushbutton 3 times and hold for 10 seconds to reset the device to the factory default mode.

TIP: In case of the 2-gang pushbutton, short press the top-right pushbutton 3 times and hold for 10 seconds to reset the device to the factory default mode.
NOTE: All configuration data, user data and network data are deleted.

QR code for this page

Was this helpful?