DUG_Push-button Module, 1-gang/2-gang_WH-02

Setting up a schedule

The devices can be fully controlled by schedules. Once the schedule is set, the devices operate at a given time.
To create a schedule:
  1. On the Home page, tap .
  2. Go to Schedules > to create a schedule.
  3. Enter the name of the schedule (A).
  4. In the TYPE menu, select Lights (B).
  5. In the APPLIES TO menu, select Switch (C) from the listed devices.
  6. Tap Create to setup events.
  7. Tap to add an event such as STATE (lights On/Off) and WHEN (sunrise/sunset or specific time range).
    NOTE: Tap to copy schedule from one day to other days or copy the entire schedule to a new schedule or to an existing one.
  8. Tap Set to save the schedule.
    NOTE: Follow the steps above to set a schedule for pushbutton dimmer and shutter respectively.
QR code for this page

Was this helpful?