DUG_Push-button Module, 1-gang/2-gang_WH-02

Setting the device location

Using the Wiser Home app, you can assign your 1-gang shutter to any room (such as bedroom, living room, dining room etc).
To assign a 1-gang shutter to a room:
  1. On the Home page, tap .
  2. Tap Devices > 1-Gang Shutter > Location (A) to assign the 1-gang shutter to the existing room or a new room (B) and tap Submit.
    NOTE:
    • Tap Remove from Room to remove the device from the existing room.

    • 1-Gang Shutter is the name given to the device by the user when pairing with the Wiser Hub. You can assign a name according to your shutter type. Example, Shutter slat.

QR code for this page

Was this helpful?