DUG_Push-button Module, 1-gang/2-gang_WH-02

Setting the default run time

Each shutter motor varies in the time it takes to complete the opening/closing movement (i.e., edge to edge). Therefore, the opening/closing time of the shutter must be determined in the app.
To determine the default run time, manually open/close the shutter.
  1. Record the time it takes to open/close the shutter completely.

  2. Record the time it takes to rotate the slats completely from closed to open position for shutter with tilting slats.


Follow the procedure according to your shutter type:
QR code for this page

Was this helpful?