DUG_Push-button Module, 1-gang/2-gang_WH-03

Removing the device

Using the Wiser Home app, you can remove the 1-gang dimmer from the system.
To remove the 1-gang dimmer:
  1. On the Home page, tap .
  2. Tap Devices, select the device you want to remove and then tap Delete (A).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?