DUG_Push-button Module, 1-gang/2-gang_WH-03

Setting the device location in the room

Using the Wiser Home app, you can assign your 1-gang dimmer to any room (such as bedroom, living room, dining room etc.).
To assign a 1-gang dimmer to a room:
  1. On the Home page, tap .
  2. Tap Devices > 1-gang Dimmer > Location to open setup page.
  3. On setup page, you can enter New room name (A) or select an existing room from the list (B).
    TIP: If the device is already assigned, you can remove it from the existing room. Tap Remove from Room (C).
  4. Once changes are done, tap Submit (D).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?