DUG_Push-button Module, 1-gang/2-gang_WH-03

Identifying the device

Using the Wiser Home app, you can identify a 1-gang shutter from the other available devices in the room.
To identify the 1-gang shutter:
  1. On the Home page, tap .
  2. Tap Devices > 1- Gang Shutter or Shutter slat > Identify (A).
    NOTE:
    • The status LED blinks red and the shutter opens/closes gradually, upon successful identification of the 1-gang shutter or shutter slat.

    • Tap OK to finish identifying the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?