DUG_Unica Relay Switch_WH-05

Pairing Wireless Switch with Relay Switch

  1. Remove the rocker from the Wireless switch.
  2. Short press the top-right push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  3. Short press the push-button of the Relay Switch 5 times in quick succession.
    The status LED blinks green.

    The light connected to the Relay Switch blinks for a few times. The status LED stops blinking green on the Wireless switch and the Relay Switch. The Relay Switch can now be controlled by the Wireless switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?