DUG_Unica Relay Switch_WH-07

Switching On/Off the device manually

You can turn on/off the device manually. The device powers the electrical appliances connected to it.
Short press the push button once to turn on/off the relay switch.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?