DUG_Unica Relay Switch_WH-07

Using the device

The Device Control Screen allows you to switch on/off the device and control various settings.

On the Control tab, select the relay switch.

The Device Control Screen displays the following options:

A

Tap to turn the device on/off.

B

Tap to open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule.

C

Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide.

D

Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.