DUG_Unica Relay Switch_WH-04

Pairing the device

Using the Wiser Home app, pair your relay switch with the Wiser Hub to access and control the relay switch.
  1. On the Home page, tap .
  2. Tap Devices > > Lights > 1-gang > Next.
    NOTE: The next screen shows the joining process of relay switch.
  3. Short press the push button 3 times and make sure that the LED blinks amber.

  4. Wait for a few seconds until the LED turns green. You can also see in the app that the device is joined.
    NOTE: If the LED is blinking green and red, see the instructions by tapping the link LED blinking green and red?.
  5. Tap Next to enter the name of the device and assign the device to a new room or an existing room.
    The relay switch is now listed under All devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?